Update Stimulus Definition (Component Test)
The expanding parameter group updates the definition of tones from predefined settings or from the tones used in the current measurement.
The multitone stimulus definition can be viewed in the Stimulus Definition trace.
defines stimulus tones based on Amplitude and Phase.
Amplitude specifies the amplitude of all tones (currently fixed at a constant 0 dB).
Constant Amplitude (0 dB): Constant amplitude. In this mode, the Phase parameter becomes available to define the multitone stimulus phase.
Random I/Q (0 dB): I and Q values are IID Gaussian distributed. In this mode, the DC tone is omitted when there are an odd number of tones.
Phase (only available when Amplitude = Constant Amplitude (0 dB)) specifies the phase of the multitone stimulus to apply to the tones.
Constant: Constant (0 deg) phase for all tones.
Parabolic: Parabolic phase across the tones (chirp-like)
Update updates the stimulus tone definition according to the settings.
updates the definition of tones based on the current multitone measurement. The Active/Inactive, Detection Threshold, Magnitude and Phase properties determine what properties of the tone definitions are updated. This is useful when evaluating different tone notching scenarios with a common multitone signal definition, or when switching between multiple multitone signal definitions (if the precise reference of the original signal is not required for the measurement task). This may also be useful for correcting the stimulus signal reference for impairments in the signal generator or fixturing prior to the desired measurement plane. This may significantly simplify making relative component test measurements (like group delay, phase linearity, or magnitude linearity).
This feature is not available when Support Balanced/Unbalanced/IQ Responses is enabled.
Active/Inactive determines which tones in the current definition are active or inactive based on the current measurements and the value of Detection Threshold.
specifies the tone power level (relative to peak tone power level) to consider a tone as active when auto-detecting tone active/inactive status from the measured waveform (Update operation).
When is selected, the measurement tries to automatically detect the enabled/disabled state of tones when an Update operation is performed. If selected, the variance of measured tone magnitude will determine how the update stimulus from response operation decides active or inactive state of each tone. If not selected, the Detection Threshold is used instead. When Active/Inactive parameter is not selected, this value is ignored by the update stimulus from response operation and the GUI control is disabled.
Magnitude replaces the magnitude of all tones in the multitone definition to reflect the current measurement results.
Phase replaces the phase of all tones in the multitone definition to reflect the current measurement results.
Update updates the stimulus tone definition according to the settings.
See Also