Frequency Offset (Component Test)
When selected, enables frequency offset compensation for component test measurement. When enabled, the analyzer will correct the acquired time data for frequency offset before calculating the channel response.
If the center frequency of the multitone stimulus signal varies by more than half of the tone spacing, Coarse Frequency Estimation may need to be enabled to make reliable measurements.
See Also