Compensation Tab (Component Test)

The Compensation tab enables the user to configure the channel response measurement to adjust the analysis based on anticipated or discovered differences between the stimulus signal definition and the measured response waveforms.

The Compensation tab dialog box allows you configure these parameters:

See Also

Component Test Properties Dialog Box