Polynomial Order (Component Test)

Polynomial Order determines the order of the polynomial fit used for the AM Amplitude Modulation - CW modulation using amplitude variation in proportion to the amplitude of the modulating signal. Usually taken as DSB-LC for commercial broadcast transmissions and DSB-SC for multiplexed systems.-AM / AM-PM curves. Polynomial Order is only shown in Statistical Computation Mode.

Default: 5 (range 1–20)

See Also

   Analysis Tab (Component Test)

   AM/AM trace

   AM/PM trace

   Linearity Summary trace