Linearity Summary (Component Test)
The trace is a matrix table that aggregates the AM/AM and AM/PM polynomial-fit results for every channel. The table has one column per channel — the measurement channels (, or when the reference channel differs) and the stimulus source channel ().
The rows are the polynomial-fit coefficients: AM/AM c0 through AM/AM cP (dimensionless) and AM/PM c0 through AM/PM cP, where P is the Polynomial Order setting.
The AM/PM coefficients in this table are in radians, even though the AM/PM trace itself displays degrees.
This trace is only computed when Computation Mode = Statistical.
See Also