Smoothing Interval (Component Test)

Smoothing Interval sets the drift (phase/gain) compensation smoothing interval (in seconds). The number of repetitions of the stimulus signal (periods) is calculated and displayed (grayed out) to the right.

The allowed values for this property may be quantized based on the period of the stimulus.

See Also

   Compensation Tab (Component Test)