Inst Inv Stim Impulse Response Unbal (Component Test)
is the non-averaged inverse impulse response of the stimulus source. If averaging is enabled, this trace does not show the effects of averaging. The Stimulus Source traces are good for troubleshooting (if your DUT Device under Test: An acronym used to describe some type of electrical apparatus connected to test instrumentation. The apparatus can range from a single component to a complex subsystem such as a mobile phone, base station or MSC. response traces look bad, check the Stimulus Source traces to see if the stimulus looks as expected).
For information about unbalanced inverse stimulus source impulse response, see Inv Stim Impulse Response Unbal.
See Also