Inv Stim Impulse Response Unbal (Component Test)
is the unbalanced part of the inverse stimulus source impulse response. The Stimulus Source traces are good for troubleshooting (if your DUT Device under Test: An acronym used to describe some type of electrical apparatus connected to test instrumentation. The apparatus can range from a single component to a complex subsystem such as a mobile phone, base station or MSC. response traces look bad, check the Stimulus Source traces to see if the stimulus looks as expected)
The non-averaged unbalanced inverse stimulus source impulse response is shown in the Inst Inv Stim Impulse Response Unbal trace.
See Also