Stim Eq IQ Meas (Component Test)
The trace is the equalized, source-side counterpart to IQ Meas: the stimulus source channel's measured IQ signal after the estimated linear channel response is compensated, per the EVM Equalization and Include Unbalanced in EVM Equalization controls (see Eq IQ Meas for how the two equalization choices behave).
This trace only has contents when Reference = Measured Stimulus and Computation Mode = Statistical.
See Also