Stim IQ Meas (Component Test)

The Stim IQ Meas trace is the source-side counterpart to IQ Meas: the measured, symbol-aligned IQ signal of the stimulus source channel, sampled at 2 samples per symbol with normalized (unitless) I and Q values.

This trace only has contents when Reference = Measured Stimulus.

See Also

Stim IQ Ref

Stim Error Vector Time

IQ Meas

Available Trace Data