Stim Error Vector Time (Component Test)

The Stim Error Vector Time trace is the source-side counterpart to Error Vector Time: the normalized error vector (measured minus reference), in percent, computed from the stimulus source channel's Stim IQ Meas and Stim IQ Ref signals. Use it to judge how much of the DUT Device under Test: An acronym used to describe some type of electrical apparatus connected to test instrumentation. The apparatus can range from a single component to a complex subsystem such as a mobile phone, base station or MSC. channel's error originates in the source itself.

This trace only has contents when Reference = Measured Stimulus.

See Also

Error Vector Time

Stim Eq Error Vector Time

Available Trace Data