Carrier Aggregation Tab (Custom OFDM)

The Carrier Aggregation tab configures component carriers and their channel assignments.

Aggregation combines up to 16 component carriers into a single signal. The Carrier Aggregation feature allows you to define and simultaneously analyze multiple carriers. Each carrier can have different allocations, measurement parameters, and even system rate.

The Carrier Aggregation tab configures these parameters:

Selected CC for Trace Display

Component Carriers

Cross-Correlated EVM

Acquisition Configuration

See Also

See "Component Carrier Selection (Custom OFDM)"

Custom OFDM Properties Dialog Box