Custom OFDM Demod Properties Dialog Box
The Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Demod Properties dialog box contains parameters that let you configure the VSA to demodulate user defined Custom OFDM modulated signals.
The Custom OFDM demodulator must be selected before this dialog box is available. To enable the demodulator, click .
The dialog box contains these tabs:
See Also
Selecting the Custom OFDM Demodulator
Making a Custom OFDM Measurement