EVM (dB) (Custom OFDM)
is the RMS value of the Error Vector Magnitude over the entire burst (includes, Preamble, Pilot, and Data subcarriers) expressed in decibels (dB).
EVM (%rms) is the EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. expressed as percentage of the RMS average EVM.
For more information about this parameter, see Error Vector Magnitude (Digital Demodulation).
See Also
Available Error Summary Results