Power (Custom OFDM)
is the average channel power (in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) of the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. signal and is calculated in the time domain over all symbols in the Measurement Interval, excluding any configured Time Gap (Samples) Per Symbol.
See Also
Available Error Summary Results