Measurement Interval (Custom OFDM)
specifies the how much time data (in symbols) within the Result Length that is used for measurement analysis data (computing the trace and symbol table data results). Measurement Interval is entered as an integer number of symbols. The parameter is used to position the start of the Measurement Interval data with respect to the first symbol in the measurement burst. The sum of the Measurement Interval plus Measurement Offset must fit within the measurement Result Length, see figure below.
The sum of the Measurement Interval plus Measurement Offset must fit within the measurement Result Length.
You can view the measurement analysis time date in the Time trace.
See Also
Time trace data
Custom OFDM Demodulation Properties Dialog Box