Cross Correlated EVM Summary (Custom OFDM)
There are two types of traces in the Trace > Data > Demod menu that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Carrier Aggregation > Selected CC for Trace Display parameter). See About Demod Per-Carrier Trace Types for more information.
The trace displays calculated cross-correlated EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. results when Cross-Correlated EVM is selected (true). The first row of the matrix displays the overall result. For MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. signals (more than one stream), a separate result for each stream will be shown after the overall result.
-
ccEVM - Cross-correlated EVM result (in dB).
There are various factors that can contribute to unexpected ccEVM results. To ensure a good ccEVM measurement, do the following:
- Manually limit the Syncronization Region to make sure that the two CCs are measuring the same time/frame interval
- Increase the Result Length to get more accurate symbol clock error estimation and compensation
- Turn on Symbol Clock Error Compensation
-
Valid Points - All active points except those with reference values that are different between measurements 1 and 2.
-
Total Points - All active points.
Active points are all subcarrier points in all symbols in the Measurement Interval except for those which are inactive (for example, inactive RUs or punctured bands).
Averaging
The Cross Correlated traces participate in measurement averaging (Analysis > Average) when average type is RMS or RMS Exponential. The "Vect: NNN" annotation at the top of the trace indicates that averaging is done as a complex average rather than RMS averaging ("RMS: NNN") used on other traces.
For more information on ccEVM, see Cross-Correlated EVM.
See Also