IQ Meas (Custom OFDM)

There are two types of traces in the Trace > Data > Demod menu that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Carrier Aggregation > Selected CC for Trace Display parameter). See About Demod Per-Carrier Trace Types for more information.

When Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Demodulation is selected, IQ Meas trace is the measured IQ symbol values used to calculate the EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. data results. There is one complex value for each subcarrier for each OFDM symbol in the measurement burst.

Trace Color coding Scheme

A multi-color coding scheme is used to make it easy to visually identify common symbols, subcarriers, and data results within various OFDM Traces. This makes cross trace data comparisons and analysis easy to accomplish. Different colors are assigned to symbols representing a common subcarrier type including: Preamble, Pilot, Data, and Null subcarrier types. Some common color scheme Traces include: Error Vect vs. Carrier, Error Vect vs. Sym, IQ Meas, OFDM Data Burst Info, and Symbols trace data.

You can also customize and re-assign Trace colors schemes, see the Display Preferences Color tab (click Utilities > Display Preferences > Color tab and select a new color for the active Mod Type element).

See Also

Available Trace Data