RE Power Heatmap (Custom OFDM)
displays a two-dimensional representation of Resource Element Power for the reference component carrier with measurement symbols on the X axis, carriers on the Y axis, and Power (in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) represented by color (similar to Spectrogram). See the RE Power 3D trace for a three-dimensional view of RE Power data.
See Also