Selecting Digital Demod
Menu Path:
Selecting the QAM Quadrature Amplitude Modulation or QPSK Quadrature phase shift keying.
measurement type configures the VSA to demodulate digitally modulated signals such asExample recordings
The 89600 VSA includes several example signals that can be used to help you learn how to use the Digital Demodulator. The included signals are listed in the Demo and Recorded Signals topic in the Getting Started book. Specifically, see the signals in these folders: APSK, DTV, GSM Global System for Mobile Communications: Originally developed as a pan-European standard for digital mobile telephony, GSM has become the world’s most widely used mobile system. It is used on the 900 MHz and 1800 MHz frequencies in Europe, Asia and Australia, and the 1900 MHz frequency in North America and Latin America. Edge Evo, Other, QAM, QPSK, ShapedOffsetQPSK.
See Also