Demo and Recorded Signals
The Keysight 89600 VSA software provides various demo signal packages that include: recorded signals, signal setup files, or Signal Studio setup files, and a demo help topic. The Demo signals are used to demonstrate the measurement capabilities and features of the 89600 VSA. These recorded signals are also available for you to use with a licensed 89600 VSA application.
How to Open a Demo Signal
Demo signals are used to demonstrate 89600 VSA measurements using recorded signals. Frequently used demo signals are installed with the VSA software. Less frequently used demo signals are available for download.
When you select a signal demo file, a demo description help file (.htm) will open in a browser, the recorded signal file will be loaded, and the 89600 VSA will be configured to make a measurement. To select and start a demo signal, click and navigate to the desired demo file.
File Formats
File format extensions associated with Demo, recorded signals, setup, and Signal Studio files:
- Demo Help files: *.htm
- Recorded Signals (example time capture signals): *.sdf
- VSA Setup file: *.set, *.setx
- Signal Studio setup files: *.xml
Installed Demo Signals
The following table provides a list of demo signals that are installed with the 89600 VSA Software. These files are located in the following default installation directory:
%PROGRAMFILES%\Keysight\89600 Software <ReleaseVersion>\89600 VSA Software\Help\Signals\(Signal subfolder)
|
Signal Subfolder |
Signal File Name |
Signal Description |
|---|---|---|
|
...\5G NR |
DL Down Link (forward link: from base station to cell phone)_at_3_5_GHz Gigahertz: A frequency measurement which equals one billion hertz._100_MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. |
Single component carrier generated by N7631C version 2.0.0.0. This signal contains SS/PBCH, PDCCH, and three PDSCH Physical Downlink Shared Channel (QPSK Quadrature phase shift keying, QAM16 and QAM256), the SSBlock Lmax = 4, period is 5ms, and the subcarrier spacing is 30kHz for both SS/PBCH and DLBWP. |
|
|
DL_Mixed_Numerology_30_60kHz |
Single component carrier generated by N7631C version 2.0.0.0. This signal contains SS/PBCH with 30 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second). numerology, and PDSCH (QAM64) within a DLBWP configured for 60 kHz numerology. |
|
|
PUSCH_2Ant_30kHz_Bw50M |
Single component carrier generated by N7631C version 1.1.18.0. This signal contains PUSCH, using two antenna ports with direct mapping between a two channel transmitter to a two channel analyzer. The PUSCH is configured with 256QAM and subcarrier spacing of 30 kHz. The bandwidth profile is 50 MHz with a center frequency of 3.5 GHz. |
|
|
PUSCH_BW100MHz_2Codewords_8x8MIMO |
Single component carrier 5G-Advanced signal, with 100MHz bandwidth and 30kHz subcarrier spacing. This signal contains PUSCH, using eight antenna ports with direct mapping between an eight channel transmitter to an eight channel analyzer. Two transport blocks are tranmitted on this PUSCH, transport block 1 is 64QAM and transport block 2 is QPSK. |
|
...\6GR |
6GR_FR1_40MHz |
Single 3GPP 6GR downlink component carrier generated by PWSG (Desktop) version 7.15.0-63, starting from PWSG's default 6GR configuration in FR1 with a 40 MHz channel bandwidth (106 resource blocks, 30 kHz subcarrier spacing). The signal contains PDSCH (256-QAM Quadrature Amplitude Modulation), spans 3 frames (10 subframes, 30 ms), and AWGN Additive White Gaussian Noise - Statistically random radio noise characterized by a wide frequency range with regards to a signal in a communications channel. has been added (C/N See carrier-to-noise ratio. = 45 dB). |
|
...\802_11ac |
VHT very high throughput (VHT) physical (PHY) layer protocol data unit (PPDU):A PPDU transmitted using the TXVECTOR FORMAT parameter equal to VHT._BW40_MCS4_PhaseNoise | 40 MHz single-channel 802.11ac signal. The signal has a significant phase noise impairment, making the constellation “fuzzy”. The phase noise is around -90 dBc/Hz amplitude in a 1 Hz bandwidth relative to the carrier over the range of 30 kHz to 1 MHz. |
|
|
VHT_BW80_MCS8_Nss4_50dBSNR_50dBIQOffset | 4-transmitter 80 MHz 802.11ac signal, using MCS modulation and coding scheme 8 (4 data streams on four antennas, using 256-QAM data subcarrier modulation format). |
| VHT_BW80_MU Multi-user_8x8_SE_50dBSNR | 80 MHz 8x8 MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. 802.11ac signal. The transmitter had 8 different data streams, and used spatial expansion to spread these data streams across 8 antennas. This is a multi-user 802.11ac signal, so the 8 data streams are assigned to different users. The number of users and the assignment of data streams to users varies in the different bursts in this signal. The signal has an overall SNR Signal-to-Noise Ratio of around 50 dB. | |
|
|
VHT_BW80+80_MCS8_Nss1_40dBSNR | 80+80 MHz 802.11ac signal, using MCS 8 (1 data stream on two separate frequency segments, using 256-QAM data subcarrier modulation format). |
|
|
VHT_BW160_MCS8_SEM | Single-channel 160 MHz 802.11ac VHT PPDU 1) IEEE 802.11: PHY (formerly PLCP) protocol data unit or 2) DVB-RCS2 (RLE): payload adapted PDU signal, Fc = 5.18GHz, BW = 160MHz, Modulation = MCS 8(256QAM) and demonstrates the Spectral Emission Mask, which is computed from the same data as used by the modulation analysis. |
|
...\802_11ax |
HE_BW20_MCS1_ExtendedRangeSU | Single-channel 20 MHz 802.11ax HE extended range SU Single user PPDU signal. |
|
|
HE_BW20_RU106-26-106_TriggerBased |
Single-channel 20 MHz 802.11ax HE trigger based PPDU signal. The 20 MHz band includes 3 RUs containing 106, 26 and 106 tones respectively. The state of first two RUs is off. |
|
|
HE_BW40_MCS7_Nss1_CompressionModeOn |
Single-channel 40 MHz 802.11ax OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. signal with the compression mode On. The MCS index of the only user is 7 |
| HE_BW80_RU484-26-106-26-106-106-26-106-SIGB |
Single-channel 80 MHz 802.11ax OFDM signal. The 80 MHz band includes 8 RUs (including the central RU). Those RUs contain 484, 26, 106, 26, 106, 106, 26, 106 sub-carriers respectively. Each RU contains one user, and the modulation formats applied by those users are 1024QAM, 64QAM, BPSK Binary phase shift keying - A type of phase modulation using 2 distinct carrier phases to signal ones and zeros., QPSK, QPSK, BPSK, QPSK, and QPSK respectively. |
|
| OFDM11ax-BW40-MU_MIMO_OFDMA-TX8 | 40MHz OFDMA plus MIMO 802.11ax signal. The 40 MHz band includes 8 RUs. The central RU has a single stream; all other RUs have multiple users and multiple streams. Total user number and stream number are displayed in RU Info trace. Stream number of each user and user's modulation type are displayed in Multi-User Info Trace. MIMO Chan Matrix shows each RU's MIMO channel. | |
|
...\802_11be |
11be_80M_MU_OFDMA_8ch_MIMO | IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.11be MU OFDMA signal with 80 MHz bandwidth, 6.8 GHz center frequency, and eight transmit channels. |
|
|
11be_320MHz_Puncture2_1024QAM | Single user (MU-compression mode, 1 user) signal with 320 MHz bandwidth and 1024-QAM modulation. Fc = 7.125 GHz. |
|
...\802_11bn |
11bn_20M_ELR | Single channel 20 MHz 802.11bn UHR(Ultra High Reliability) with ELR(Enhanced Long Range) based SU PPDU signal, Fc = 2.4GHz. |
|
|
11bn_80M_MU_UEQM_4stream | IEEE 802.11bn MU OFDMA signal with 80 MHz bandwidth, 6.8 GHz center frequency, and four transmit channels. The allocation signaling for band 0 is 000011001, which corresponds to three RU/MRU allocations: 106, 26, and 106, all within the 20 MHz band 0. The signalings for band 1/2/3 are 00100000, which corresponds to one big allocation(242) within the 20 MHz band. The allocation for band 0 contains three users, UEQM is enabled for the first user. the allocation for band 1/2/3 contains one user per RU/MRU. |
|
|
11bn_160M_MU_PPDU_MCS8_SEM | Single-channel 160 MHz 802.11bn UHR(Ultra High Reliability) with based MU PPDU signal, Fc = 2.412GHz, BW = 160MHz, Modulation = MCS 8(256QAM), Punctured Channel Value = 4(111x1111) and demonstrates the Spectral Emission Mask, which is computed from the same data as used by the modulation analysis. |
|
|
11bn_160M_TB_DRU | Single user Trigger-Based PPDU with distributed Resource Units (dRU) 11bn signal, bandwidth is 160 MHz and modulation format is 256-QAM. The first RU is enabled. Fc = 6.8 GHz. |
|
|
11bn_320M_non-OFDMA_MCS20_2xLDPC | IEEE 802.11bn multiple user signal with 320 MHz bandwidth and 16-QAM modulation. The punctured channel indication is 1x111111, which indicates that the second 40 MHz segment is not used (no power), the PPDU MCS is 20 and 2xLDPC is enabled. Fc = 6 GHz. |
|
...\Adjacent Channel Power |
5GNR_TM1p1_FR1_FDD Frequency Division Duplex: A duplex scheme in which uplink and downlink transmissions use different frequencies but are typically simultaneous._4CC_CA 1) Channel Assignment or, 2) Carrier Aggregation_100M | Example of 5GNR FDD multi-carrier Adjacent Channel Leakage Power Ratio (ACLR Adjacent Channel Leakage Ratio - A measure of transmitter performance for W-CDMA. It is defined as the ratio of the transmitted power to the power measured after a receiver filter in the adjacent RF channel. This is what was formerly called Adjacent Channel Power Ratio. ACLR is specified in the 3GPP W-CDMA standard.) measurement. Four contiguous component carriers, each 100MHz wide, are aggregated and the signal configuration is based on NR FR1 test model 1.1 (NR-FR1-TM1.1) as defined in 3GPP TS Technical Specification 38.141 specification. |
|
|
5GNR_TM1p1_FR1_FDD_100M |
Example of how to make an Adjacent Channel Power (ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power.) measurement configured to match the requirements for a 5GNR 100 MHz ACLR test case. |
|
...\AdvancedRadar |
ARadar_4Emitters_4TunedFrequencies_4Tables_SegCap | Advanced Radar signal, captured using variable length segment capture, contains 4 emitters at 4 frequencies and an Advanced Radar setup that separates the 4 emitters and fills 4 pulse tables with pulse measurements. |
|
|
ARadar-3Ch-3Pulse-3Chirps |
Example showing synchronization and detection over the linear chirp domain, with the addition of pulse detection. This signal has 3 channels with identical data feeding through them. The data consides of pulses with 3 linear chirps inside them. |
|
|
ARadar-MultiFM-Pulses |
Example showing synchronization and detection over the frequency domain, with the addition of pulse detection. This signal consists of pulses with with up to 12 frequency regions inside them. |
|
...\AM Amplitude Modulation - CW modulation using amplitude variation in proportion to the amplitude of the modulating signal. Usually taken as DSB-LC for commercial broadcast transmissions and DSB-SC for multiplexed systems. FM Frequency Modulation PM |
50PCAM |
AM signal; 50% amplitude modulated by a 25 kHz sine wave with a 5 MHz RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). carrier. |
|
|
AMPMSQR |
Carrier signal Amplitude Modulated by a square wave |
|
|
AMPMTRI |
Triangle wave, Fc = 5MHz, Span = 156.25kHz |
|
|
XMITTER |
Recording of a FM transmitter turning on. The recording was allowed to play and then paused when the carrier appeared. |
|
...\ccEVM |
5GNR_DL_100MHz_ccEVM |
Modified test model signal (NR-FR1-TM1.2), generated using a single channel of an M9384B VXG. Ch1 of the VXG was connected to Ch1 and Ch2 of an S-Series oscilloscope using a power splitter. The bandwidth profile is 100 MHz with a center frequency of 2.1 GHz. |
|
...\ChannelSounding |
ChannelSounding_60GHz_L128_2ft_separation |
Channel Sounding signal that has been captured by the 89600 VSA from the following setup: signal generator; upconverter to 60 GHz band; horn antenna; open air channel (office environment with cubicles); 2 ft separation between antennas; horn antenna; 60 GHz downconverter; signal analyzer, and 89600 VSA. |
|
...\ComponentTest |
componenttest-mpath |
Component Test Measurement multi-tone signal with 100 tones spaced at 999 KHz. The signal is passing through a cabled setup with two equal paths - one path is 20 cm in length, the second path is 4 meters. This gives a path difference of 3.8 meters. |
|
...\Custom Ofdm |
CustomOFDM_5G_PDSCH_PDCCH_2x2MIMO |
5G Downlink 2x2 MIMOsignal with the following characteristics: 2x2 MIMO transmission type Center frequency = 3.5, GHz Bandwidth = 100 MHz (273 RBs), Symbol Count in Resource Map = 14 Symbols, CP 1) Contention period, or 2) Cyclic prefix Length Mode = Normal CP mode defined in 5GNR |
|
|
CustomOFDM_5G_PXSCH_8x8MIMO |
5G Downlink 8x8 MIMOsignal with the following characteristics: 8x8 MIMO transmission type, Center frequency = 3.5 GHz, Bandwidth = 100 MHz (273 RBs), Symbol Count in Resource Map = 14 Symbols, CP Length Mode = Normal CP mode defined in 5GNR |
|
|
CustomOFDM_5G_PXSCH_SISO |
3GPP 5G NR PXSCH signal with 256 QAM format; Fc = 3.5 GHz, Span 96 MHz. |
|
|
CustomOFDM_5G_SSB_PDSCH_PDCCH_SISO |
5G Downlink SISO signal with the following characteristics: Center frequency = 28 GHz, Bandwidth = 100 MHz (273 RBs), Symbol Count in Resource Map = 42 Symbols (Resoure Map repeats from symbol 28), CP Length Mode = Normal CP mode defined in 5GNR, Symbol Phase Compensation is enabled and the compensation frequency is 28GHz, Result Length = 140 symbols (10 slots) |
|
|
CustomOFDM_80211a |
IEEE std 802.11a/g OFDM signal with 64 QAM format; Fc = 5.805 GHz, Span 31.25 MHz. |
|
...\CustomIq |
24qam |
24qam is a QAM signal with a 24 point constellation format. |
|
|
BOC52 |
BOC52 is a Binary Offset Carrier (BOC) signal with rate 2 and rate 5 carriers. The symbol rate is 10.23 MHz. In the spectrum you can see the BOC subcarriers at +/- 5 MHz and +/- 15 MHz. |
|
|
GPS-L1 is is a GPS L1 signal with the 1.023 Mchip C/A code on the horizontal axis and the 10.23 Mchip P code on the vertical axis. |
|
|
|
v29-8qam |
v29-8qam is an 8PSK signal with the constellation format specified by the V.29 BIS standard. |
|
|
VSA |
VSA is a custom signal with the constellation format formed from the characters V S A. |
|
...\DvbRcs2 |
RCS2_3Sections_4Bursts_SNR34dB_BER Bit Error Ratio - A ratio of the number of errors to data bits received on a digital circuit. |
DVB-RCS2 signal with 3 time slot sections containing 4 bursts total. Section 0: Waveform ID 1 (QPSK, Rate 1/3, 664 symbols), repeated once (2 bursts). Section 1: Waveform ID 18 (8-PSK Phase Shift Keying: A broad classification of modulation techniques where the information to be transmitted is contained in the phase of the carrier wave., Rate 2/3, 1616 symbols), no repetition (1 burst). Section 2: Waveform ID 22 (16-QAM, Rate 5/6, 1616 symbols), no repetition (1 burst). Payload data is all 1s. Turbo decoding is enabled. BER measurement is enabled. SNR is 34 dB. |
|
...\DVBS2X |
DVB_QPSK_1Per3_PN9_SNR28dB |
DVBS2/X signal which is configured in Keysight Signal Studio for DVBS2X. This is an example of DVBS2/X BER test with Deinterleaver/LDPC low-density parity check Decoding/BCH Broadcast Channel Decoding/BBFrame Descrambling/BBFrame Header Decoding. The symbol rate is 20MHz, filter roll factor is 0.25, the MODCOD is QPSK1/3, and the payload bit sequence is PN9, the SNR is 28dB. |
|
|
DVB_QPSK_2Per5_PN9_SNR15dB |
DVBS2/X signal which is configured in Keysight Signal Studio for DVB-S2/S2X. This is an example of DVBS2/X BER test with Deinterleaver/LDPC Decoding/BCH Decoding/BBFrame Descrambling/BBFrame Header Decoding. The symbol rate is 20MHz, filter roll factor is 0.25, the MODCOD is QPSK2/5, and the payload bit sequence is PN9, the SNR is 15dB. |
|
|
DVBS2X_256APSK_128_180 |
DVB-S2X signal which is configured in Keysight Signal Studio for DVB-S2/S2X. This is an example of DVB-S2X EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format./BER test with Deinterleaver/LDPC Decoding/BCH Decoding/BBFrame Descrambling/BBFrame Header Decoding. The symbol rate is 20MHz, filter roll factor is 0.25, the MODCOD is 256APSK128/180, and the payload bit sequence is PN9, the SNR is 44dB. |
|
...\FlexFrame |
8PSKPreamble64QAMData |
Example of a periodic type signal with a 1 GHz symbol rate and centered at 4 GHz. The signal has a preamble at the beginning of the frame, which has a PN9 payload type and a 8 PSK modulation type. The second segment in this signal is data segment and uses the 64 QAM modulation format. |
|
|
802_15_3d |
Example of a 7.04GHz sample rate, scrambled 802.15.3d signal centered at 307 GHz. It shows how Flex Frame can be used to measure SYNC, SFD Start frame delimiter, CES, and Payload portions of 802.15.3d signal. The signal was generated using Keysight Signal Studio for Custom IQ. |
|
|
80211ad_SC_Data |
Example of a burst type 1.76GHz sampled rate 3.52 GHz bandwidth 802.11ad signal with 40 dB SNR and 100 kHz frequency offset. |
|
|
80211ay_Ncb2 |
Example of a 3.52 GHz sample rate, burst type 802.11ay signal centered at 10.5 GHz. It shows how multi-carrier support in Flex Frame can be used to measure pre-EDMG Lowband, pre-EDMG Highband, and EDMG that are centered at 9.42, 11.58, and 10.5 GHz, respectively. |
|
|
80211ay_Ncb2_EDMG |
Example of a 3.52 GHz sample rate, burst type 802.11ay signal centered at 10.5 GHz with 40 dB SNR and 100 kHz frequency offset. It shows how Flex Frame can be used to measure EDMG-STF, EDMG-CEF, guard interval, and data portions of the 802.11ay signal. |
|
|
80211ay_Ncb2_preEDMG_Highband |
Example of a 3.52 GHz sample rate, burst type 802.11ay signal centered at 10.5 GHz with 40 dB SNR and 100 kHz frequency offset. It shows how Flex Frame can be used to measure high-frequency band of pre-EDMG modulated fields, namely L-STF Non-HT Short Training field, L-CEF, L-Header, and EDMG-Header-A portions of the 802.11ay signal. |
|
|
80211ay_Ncb2_preEDMG_Lowband |
Example of a 3.52 GHz sample rate, burst type 802.11ay signal centered at 10.5 GHz with 40 dB SNR and 100 kHz frequency offset. It shows how Flex Frame can be used to measure low-frequency band of pre-EDMG modulated fields, namely L-STF, L-CEF, L-Header, and EDMG-Header-A portions of the 802.11ay signal. |
|
|
DVB_RCS2_Reference_Waveform_ID2_for_LM_Burst_2CC |
Example of a hardware generated 2 MHz sample rate DVB-RCS2 signal with two component carriers centered at 1 GHz and 1.0025 GHz. The waveform sent over each component carrier is based on the reference waveform ID2 given in Table A-1 in ETSI European Telecommunications Standard Institute: The European standardization body for telecommunications. EN 301 545-2 V1.2.1. It shows how Flex Frame can be used to measure preamble, data, pilot, and postamble portions of the each component carrier of the DVB-RCS2 signal. The signal was configured using Keysight Signal Studio for Custom Modulation and generated with the hardware. |
|
|
Hw_generated_DVB_S2X_64_APSK_8_16_20_20_rate_7_per_9 |
Example of a 1 MHz sample rate, hardware generated DVB-S2X signal centered at 1 GHz. It shows how Flex Frame can be used to measure SOF, PLSCODE, data, and pilot portions of the DVB-S2X signal. The signal was generated using Keysight Signal Studio for Digital Video. |
|
|
Ideal_DVB_S2X_32_APSK_4_12_16_rate_2_per_3 |
Example of a 1 MHz sample rate, ideal DVB-S2X signal centered at 1 GHz. It shows how Flex Frame can be used to measure SOF, PLSCODE, data, and pilot portions of the DVB-S2X signal. The signal was generated using Keysight Signal Studio for Digital Video. |
|
|
MixedModulation |
Example of a periodic type signal with a 1 GHz symbol rate and centered at 4 GHz. The signal has a synchronization field at the beginning of the frame, which has a PN9 payload type and a BPSK modulation type. The hannel estimation field (CEF) uses the QPSK modulation format. The remaining data segments are modulated with the available modulation formats in FlexFrame. |
|
|
QPSKPreamble16QAMData |
Example of a periodic type signal with a 1 GHz symbol rate and centered at 4 GHz. The signal has a preamble at the beginning of the frame, which has a PN9 payload type and a QPSK modulation type. The second segment in this signal is data segment and uses the 16 QAM modulation format. |
|
|
Scrambled_DVB_S2X_8_APSK_2_4_2_rate_100_per_180 |
Example of a 1 MHz sample rate, scrambled DVB-S2X signal centered at 1 GHz. It shows how Flex Frame can be used to measure SOF, PLSCODE, data, and pilot portions of the scrambled DVB-S2X signal. The signal was generated using Keysight Signal Studio for Digital Video. |
|
...\FMCW Radar |
FMCW_140MHzDeviation_50_5_50_5usec_UpCwDnCwChirp |
Example of a repeating FMCW modulation signal pattern consisting of multiple repeating Linear FM (LFM) Up-Down-chirps. |
|
|
FMCW_140MHzDeviation_90usec_UpChirp |
Example of a repeating FMCW modulation signal pattern consisting of multiple repeating Linear FM (LFM) Up-chirps. |
|
...\HrpUwb |
HrpUwb_Ch9_Code10_L4_Sync64_Sfd8_33octet |
This signal conforms to section 15 of the IEEE 802.15.4-2020 standard. The SHR portion of the signal is defined as: Channel = 9 (Center frequency = 7987.2 MHz, Pulse bandwidth = 499.2 MHz), PHY Physical Layer Mode = Non-ERDEV, Code Index = 10, Delta Length = 4, SYNC Length = 64 and SFD Length = Short (8). The PHY payload data is defined as: Hop Bursts = 2, Chips per Burst = 8, Frame Length = 33 octets (including CRC Cyclic Redundancy Check). |
|
...\LTE |
LTE_FDD_DL_5MHz_2x2_Encoded_v890 |
This is an LTE FDD Downlink 2x2 MIMOsignal |
|
|
LTE_FDD_DL_5MHz_4x4_Impair_v860 | This is an impaired LTE FDD downlink 4x4 MIMO signal |
|
|
LTE_FDD_UL Up Link (reverse link: from cell phone to base station)_5MHz_v860 |
Signal conforms to v 8.6.0 (March 2009) of 3GPP LTE Standard (TS 36.211). |
| LTE_FDD_UL_5MHz_Encoded_v890 | This is a 5 MHz Uplink LTE FDD signal, whose PUSCH and PUCCH are encoded with UCI Information; Fc = 1GHz, Span = 6 MHz. | |
|
|
LTE_FDD_UL_5MHz_PRACH Physical Random Access Channel_v860 |
Signal conforms to v 8.6.0 (March 2009) of 3GPP LTE Standard (TS 36.211). LTE_FDD_UL_5MHz_PRACH_v860 is a 5 MHz Uplink LTE FDD signal consisting of only PRACH. |
|
|
LTE_FDD_UL_5MHz_v860 | This is a 5 MHz Uplink LTE FDD signal consisting of PUSCH, PUCCH and SRS; Fc = 1GHz, Span = 5 MHz (25 RB). |
|
|
LTE_TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period._DL_5MHz_4Ant_Beamforming_v890 | This is an LTE TDD signal is a downlink 4-antenna beamforming with UE User Equipment (e.g. cell phone)-specific RS signal |
|
|
LTE_TDD_DL_5MHz_4x2_WithChannel_v890 | This is a 4-antenna port 5 MHz Downlink LTE TDD signal consisting of PDSCH precoded with Spatial Multiplexing for 2 layers, and passed through a simulated wireless fading channel |
|
|
LTE_TDD_DL_5MHz_Encoded_v890 | This is an LTE TDD downlink fully encoded control channel signal |
|
|
LTE_TDD_DL_5MHz_v860 |
Signal conforms to v 8.6.0 (March 2009) of 3GPP LTE Standard (TS 36.211). LTE_TDD_DL_5MHz_v860 is a single antenna 5 MHz Downlink LTE TDD signal. |
|
|
LTE_TDD_UL_5MHz_PRACH_v860 |
Signal conforms to v 8.6.0 (March 2009) of 3GPP LTE Standard (TS 36.211). LTE_TDD_UL_5MHz_PRACH_v860 is a 5 MHz Uplink LTE TDD signal consisting of only PRACH. |
|
|
LTE_TDD_UL_5MHz_v860 |
Signal conforms to v 8.6.0 (March 2009) of 3GPP LTE Standard (TS 36.211). LTE_TDD_UL_5MHz_v860 is a 5 MHz Uplink LTE TDD signal consisting of PUSCH, PUCCH and SRS. |
|
...\LTE-A |
LTEA-FDD-2CC-CrossCarrierScheduling |
This is an LTE-Advanced FDD signal with the following characteristics:
|
|
|
LTEA-FDD-5MHz-TM9-8x8 |
This is an LTE-Advanced FDD signal with the following characteristics:
|
|
|
LTEA-FDD-DL-5M5M5M-Inter-band-CA |
LTE-Advanced FDD Downlink signal demonstrating Interband Carrier Aggregation. 3 component carriers
|
| LTEA-FDD-DL-5M10M |
Downlink FDD LTE-Advanced Downlink signal. 2 component carriers
Center frequency = 2.14 GHz |
|
| LTEA-FDD-UL-3M5M |
Uplink FDD LTE-Advanced signal. 2 component carriers
Center frequency = 2.14 GHz |
|
| LTEA-TDD-DL-1P4M3M5M |
Downlink TDD LTE-Advanced signal. 3 component carriers
Center frequency = 2.35 GHz |
|
| LTEA-TDD-UL-5M10M |
Uplink TDD LTE -Advanced signal. 2 component carriers
Center frequency = 2.35 GHz |
|
|
...\Multi-Measurement |
Four measurement setup configured to demodulate LTE, W-CDMA Code Division Multiple Access: One of several digital wireless transmission methods in which signals are encoded using a specific pseudo-random sequence, or code, to define a communication channel. A receiver, knowing the code, can use it to decode the received signal in the presence of other signals in the channel. This is one of several "spread spectrum" techniques, which allows multiple users to share the same radio frequency spectrum by assigning each active user an unique code. CDMA offers improved spectral efficiency over analog transmission in that it allows for greater frequency reuse. Other characteristics of CDMA systems reduce dropped calls, increase battery life and offer more secure transmission. See also IS-95., and GSM carriers as well as a Vector measurement to show an overall spectrum and CCDF Complementary Cumulative Distribution Function. |
|
|
|
LTE_WCDMA_GSM_Sequence |
Multi-carrier signal containing the following formats:
|
|
...\NB-IoT |
NBIoT_DL_InBandDiffPci_10MHz |
Downlink NBIoT signal that is inserted into the middle of a 10 MHz LTE carrier. One user transmission is defined. NPDCCH is transmitted in subframes 1 and 2 and NPDSCH is transmitted in slots 12 and 13. |
|
|
NBIoT_DL_StandAlone |
Downlink NBIoT signal with 1.92Msps sampling rate. Two user transmissions are defined. NPDCCH is transmitted in subframes 1 and 2. NPDSCH is transmitted in slots 12 and 13 for User01 and slots 16, 17, 22-29, and 32-37 for User02. |
|
|
NBIoT_UL_NPRACH_12T_8Rep |
Uplink NB-IoT signal containing an NPRACH burst with 12 tones and an offset of 18 subcarriers. The format is Format 0 and there are 8 repetitions of the symbol group sequence. Format 0 contains five symbols per symbol group. |
|
|
NBIoT_UL_NPUSCH_1T_2RU_2Rep |
Single-tone uplink NB-IoT signal containing an NPUSCH burst that is two RU long with two repetitions. MCS is 3 and modulation is pi/4 QPSK. The subcarrier spacing is 15 kHz and the offset is 6 subcarriers. |
|
...\Pulse |
Pulse_1_2_3_4usecWidth_1msPRI_ |
This is a low duty cycle, Continuous Wave (CW) pulsed, frequency hopping signal. |
|
|
Pulse_5usecWidth_10usPRI_FreqHop_Barker |
This is a high duty cycle, pulsed, frequency hopping signal, with BPSK modulation using Barker sequences. |
|
|
Pulse_10_20_30_40usecWidth_50usecPRI_ |
This is a high duty cycle, Linear FM (LFM) pulsed, frequency hopping signal. |
|
|
Pulse_10_20_30_40usWidth_50usPRI_FreqHop_TriangleChirps |
This is a high duty cycle, pulsed, frequency hopping signal modulated by triangular chirps. |
|
|
Pulse_AoA_4ch_Tdoa |
Pulse Angle of Arrival is a measurement that calculates the direction (angle) from which a signal is received. To perform this measurement, you need at least 2 channels to calculate the angle. This signal was constructed with 4 antennas that are spaced roughly 10 meters apart from each other. |
|
|
Pulse_Deinterleaving |
Example of how to use the pulse deinterleaving feature to separate various emitters in a complex sequence of pulses. The signal was constructed as an alternating sequence of three pulses: A CW pulse at 2 GHz of 30 µs pulse with an amplitude of 1.6 dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer. A linear FM pulse at 2.01 GHz of 5 µs pulse with an amplitude of -13.45 dBm. A BPSK encoded pulse at 1.995 GHz of 10 µs pulse with an amplitude of -23.4 dBm. |
|
|
Pulse_Hopping |
This pulse hopping analysis example leverages the frequency switching analysis algorithms in the pulse measurement extension of the VSA. The signal was constructed as a series of pulses with stepped but arbitrary hops in frequency, ranging from -30 MHz to +30 MHz, using Signal Studio's Pulse Builder program. |
|
|
Pulse_Mixed_Modulation |
This is a high duty cycle, pulsed, frequency hopping signal modulated by continuous wave, linear chirps, triangular chirps and Barker-coded BPSK. |
|
|
Pulse_Scoring |
This Pulse Scoring example demonstrates the pulse similarity scoring feature. The user must define reference pulses based on the following figures of merit: top amplitude, pulse width, pulse repetition interval (PRI) and mean frequency. TThe measured pulses are then compared against this reference group of pulses, and checked for similarity. |
|
|
Pulse_Time_Sidelobe |
In this example, one main pulse with a pulse width of 30 µs is intended to be the outgoing pulse. There is one interfering pulse with an LFM chirp, and a series of other pulses intended to emulate ground clutter. |
|
|
Pulse_Train_Scoring |
Example of the Pulse Pattern Search/Train Scoring feature, used to identify and mark the locations of pulse train patterns rather than individual pulses. |
|
...\SpectralEmissionsMask |
SEM_80211BE_160MHz |
Example of how to make a Spectral Emissions Mask (SEM) measurement configured to match the requirements for an IEEE 802.11be 160 MHz test case. |
|
...\Stimulus Response |
Stim_Response_2Ch |
The Stim_Response_2Ch signal is a 2 channel signal captured through two parallel paths, Fc @ 2.1GHz, Span @ 8MHz, -15dBm and -3dBm. The setup file included with this signal demonstrates the AM/AM, AM/PM, and Gain Compression traces using the first channel as the stimulus data and the second channel as the response data. |
Downloadable Demo Signals
The following table provides a list of downloadable demo signals for use with the 89600 VSA Software. Clicking a link downloads a .zip file that contains the listed demo signals for the signal type. Unzip the file to the location of your choice, or to the VSA software installation directory path (default is %PROGRAMFILES%\Keysight\89600 Software <ReleaseVersion>\89600 VSA Software\Help\Signals) if you want to add the downloaded demo signals to the collection of installed demo signals (may require administrator privileges).
|
Signal Type/Link |
Signal File Name |
Signal Description |
|---|---|---|
|
1xEVDOFwd |
Standard 3GPP2 1xEV-DO forward link signal; Fc = 2.2GHz, Span = 1.5 MHz. |
|
|
|
1xEVDORev |
Standard 3GPP2 1xEV-DO reverse link signal; Fc = 2.2GHz, Span = 1.5 MHz. |
|
80211a_64QAM |
IEEE std 802.11a/g OFDM signal with 64 QAM format; Fc = 5.805 MHz, Span 31.25 MHz. |
|
|
|
80211b-Barker1 |
IEEE std 802.11b signal with Barker1 burst type and DBPSK Differential binary phase shift keying modulation for 1 Mbps; Fc = 2.412 MHz, Span 34.375 MHz. |
|
|
80211b-CCK11-short |
IEEE std 802.11b signal with CCK complementary code keying and short PLCP Physical layer convergence protocol header burst type and QPSK modulation for 11 Mbps; Fc = 2.412 MHz, Span 34.375 MHz. |
|
|
80211g-PBCC22-short |
IEEE std 802.11b signal with PBCC22 and short PLCP header burst type and 8PSK modulation for 22 Mbps; Fc = 2.412 MHz, Span 34.375 MHz. |
|
20 MHz HT high throughput-mixed 802.11n signal, using MCS 15 (which means 2 data streams, each using 64-QAM data subcarrier modulation format). |
||
|
|
80211n-MCS15-40MHz-GF |
40 MHz HT-greenfield 802.11n signal, using MCS 15 (which means 2 data streams, each using 64-QAM data subcarrier modulation format). |
|
|
80211n-MCS31-40MHz-MM-SE |
4-ch MIMO, 40 MHz HT-mixed 802.11n signal, using MCS 31 (4 data streams, each using 64-QAM data subcarrier modulation format). Spatial Expansion is used. |
|
APSK_128_zero |
APSK_128_zero Signal is a 128 APSK signal with a state at the origin. |
|
|
|
APSK32_9_10 |
32 APSK example recording with 9/10 coding rate (no Header or Pilot slots). This signal works with "Digital Video > DVB 32APSK > Code Rate 9/10" standard preset in AYA Digital Demod Analysis. |
|
docsis3.1-1024qam-ber |
This DOCSIS 3.1 Downstream Signal is a standard OFDM Downstream signal compatible with the physical layer specification in the CableLabs DOCSIS 3.1 specification CM Cubic Metric-SP-PHYv3.1. It has an FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. size of 4096 and a bandwidth of 96 MHz with coded PLC, NCP, and data code words in 1024 QAM. On the constellation display you will see the data subcarriers with 1024 QAM modulation, the pilot subcarriers in boosted BPSK, the preamble subcarriers in BPSK, and the PLC data subcarriers in 16 QAM. | |
|
|
docsis3.1-ds |
This DOCSIS 3.1 Downstream Signal is a standard OFDM Downstream signal compatible with the physical layer specification in the CableLabs DOCSIS 3.1 specification CM-SP-PHYv3.1-I01-131029. It has an FFT size of 4096 and a bandwidth of 95 MHz and a burst of 128 OFDM symbols. On the constellation display you will see the data subcarriers with 256 QAM modulation, the pilot subcarriers in boosted BPSK, the preamble subcarriers in BPSK, and the PLC data subcarriers in 16 QAM. There is an exclusion band in the upper part of the spectrum. |
|
|
docsis3.1-ds-4k-4p-vbl |
This DOCSIS 3.1 Downstream Signal is a standard OFDM Downstream signal compatible with the physical layer specification in the CableLabs DOCSIS 3.1 specification CM-SP-PHYv3.1. It has an FFT size of 4096 and a bandwidth of 150 MHz. There are four active profiles:
|
|
|
docsis3.1-us |
This DOCSIS 3.1 Upstream Signal is a standard OFDM Upstream signal compatible with the physical layer specification in the CableLabs DOCSIS 3.1 specification CM-SP-PHYv3.1-I01-131029. It has an FFT size of 2048 and a bandwidth of 95 MHz. The data subcarriers are modulated with 2048 QAM. The signal uses pilot pattern index 2 and spans mini-slots 0 to 235. |
|
|
docsis3.1-us-ber |
This DOCSIS 3.1 Upstream Signal is a standard OFDM Upstream signal compatible with the physical layer specification in the CableLabs DOCSIS 3.1 specification CM-SP-PHYv3.1-I01-131029. It has an FFT size of 2048 and a bandwidth of 125 MHz. The data subcarriers are modulated with 4096 QAM. The signal uses pilot pattern index 1 and spans mini-slots 0 to 49. BER Analysis is enabled and the Randomization Seed is set to 3FFFFF (Hex). |
|
DTV8_MTW |
This is a live broadcast HDTV signal with VSB8 modulation, in accordance with the North American ATSC standard. Center frequency is 749 MHz (UHF Ultra High Frequency: The RF spectrum between 300 MHz and 3 GHz. channel 60). This signal was recorded off the air, and thus shows a slightly worse signal to noise ratio (i.e., higher EVM) than would be typical for a measurement performed directly at the transmitter output. |
|
|
Edge_5Mhz |
Standard EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.)(3p/8 8PSK) "Enhanced Data for Global Evolution" digital modulated signal; Fc = 5 MHz, Span 625 kHz.
|
|
|
|
EDGEEvo_HSR_Wide_Mixed |
EDGEEvo_HSR_Wide_Mixed signal uses the “high” symbol rate, and contains time slots alternating between QPSK, 16QAM, and 32QAM. This signal uses the wide EDGE pulse-shaping filter. |
|
|
EDGEEvo_NSR_AQPSK_0.3333 signal | The EDGEEvo_NSR_AQPSK_0.3333 signal configuration uses the “normal” symbol rate, and the Alpha-QPSK modulation format with an alpha equal to 0.3333 3 (subchannel power imbalance ratio equal to -9.542 dB). |
|
|
EDGEEvo_NSR_Mixed |
EDGEEvo_NSR_Mixed signal uses the "normal" symbol rate, and contains time slots alternating between GMSK, 8PSK, 16QAM, and 32QAM |
|
|
gsm |
gsm signal is a pulsed, standard GSM format signal. |
|
Barker7Coded_Pulse |
This is a legacy demo that was created before the BHP FMCW Radar and BHQ Pulse Analysis options were available. It uses only vector mode. The signal is a pulsed radar signal with binary phase modulation on the pulse. |
|
|
|
Linear_FM_chirp |
This is a legacy demo that was created before the BHP FMCW Radar and BHQ Pulse Analysis options were available. It uses only vector mode. The signal is a pulsed radar signal with linear FM modulation, also known as chirp, on the pulse. |
|
2Ch-RF |
RF signal captured through two parallel paths, Fc @ 5.805GHz, Span @ 36MHz, -5dBm and -45dBm. |
|
|
|
2Ch-RF-Noisy |
Same as the 2Ch-RF.sdf recording above, with lower SNR. |
|
|
Dect |
This is a standard DECT Digital European Cordless Telecommunications format signal. |
|
|
nadc |
This is a pulsed, standard NADC North American Digital Cellular format signal. |
|
|
pdc |
|
|
|
phs |
This is a non-pulsed, standard PHS 1) Personal Handy Phone System, or 2) payload header suppression: The process of suppressing the repetitive portion of payload headers at the sender and restoring the headers at the receiver.(PHP Personal Handy Phone: The mobile hand-set used with the Japanese Personal Handy Phone system.) format signal. |
|
SINEWPN |
This is a 5 MHz sine wave with phase noise. |
|
|
Pre5G_1CC |
This is a single component carrier signal generated at 28 GHz using Keysight N7630C software for waveform creation. |
|
|
128QAM |
128QAM digital modulated signal; Fc @ 2 GHz, Span @ 37.1 MHz, 31.25 MHz SymbolRate, RRC measurement filter with alpha = 0.18. This signal has a high EVM due to an incorrect filter setting. To ensure successful demodulation, make sure is long enough or is turned off. |
|
|
|
Qam1024 |
This is a 1024-QAM signal. |
|
|
Qam512 |
This is a 512-QAM signal. |
|
|
Star32QAM |
This is 5 MHz Star32QAM signal with a root raised cosine measurement filter, raised cosine reference filter, an alpha of 0.35, and default ring ratios. To view this StarQAM signal, recall the Star32QAM.set setup file, then recall the Star32QAM.sdf signal file, and start the demodulator. |
|
BSTIMING |
5 MHz pulsed carrier with QPSK modulation. Symbol rate is 50 kHz, filtering is root raised cosine, and filter alpha is 0.35. This signal is similar to the QPSK.DAT recording, though that signal is not pulsed. |
|
|
|
BSTQPSK |
5 MHz pulsed carrier with π/4 shifted QPSK modulation. Symbol rate is 50 kHz, filtering is root raised cosine, and filter alpha is 0.35. This signal is similar to the BSTIMING.DAT recording, except for the π/4 shift in the modulation. |
|
|
GATE2BUR |
5 MHz pulsed carrier with two TDMA Time Division Multiple Access: A technology for digital transmission of radio signals between, for example, a mobile telephone and a radio base station. In TDMA, the frequency band is split into a number of channels which in turn are stacked into short time units so that several calls can share a single channel without interfering with one another. Networks using TDMA assign 6 timeslots for each frequency channel. TDMA is also the name of a digital technology based on the IS-136 standard. TDMA is the current designation for what was formerly known as D-AMPS. (time division multiple access) bursts. Both bursts are QPSK modulated at 50 ksymbols/second, and are root raised cosine filtered with an alpha of 0.35. The first burst is modulated with a random bit stream with an equalization sequence in the middle. The second burst is 10 dB lower that the first and modulated with a bit pattern of 8 ones and 8 zeros. |
|
|
OffsetQPSK |
Unimpaired offset QPSK (OQPSK Offset Quadrature Phase Shift Keying: A type of QPSK modulation that offsets the bit streams on the I and Q channels by a half bit. This reduces amplitude fluctuations and helps improve spectral efficiency.) signal modulated at 24.3 ksymbols/second, root raised cosine filtered with an alpha of 0.35. Another root raised cosine filter is used in the measurement process, resulting in raised cosine filtering and zero inter-symbol interference (ISI Inter-Symbol Interference: An interference effect where energy from prior symbols in a bit stream is present in later symbols. ISI is normally caused by filtering of the data streams.). |
|
|
QPSK |
QPSK modulated signal at 50 ksymbols/second, root raised cosine filtered with an alpha of 0.35.
|
|
|
QPSKALFA |
QPSK modulated signal at 50 ksymbols/second, root raised cosine filtered with a filter alpha 0.2 instead of 0.35.
|
|
|
QPSKCOMP |
QPSK modulated signal at 50 ksymbols/second, root raised cosine filtered with an alpha of 0.35 with compression errors.
|
|
|
QPSKIBAL |
QPSK modulated signal at 50 ksymbols/second, root raised cosine filtered with an alpha of 0.35 with a 1 dB gain difference between the I and Q channels.
|
|
|
QPSKIOFF |
QPSK modulated signal at 50 ksymbols/second, root raised cosine filtered with an alpha of 0.35 with -22 dB Offset error.
|
|
|
QPSKNQST |
QPSK modulated signal at 50 ksymbols/second, Nyquist (or raised cosine) instead of a root-raised cosine filtering with an alpha of 0.35.
|
|
|
QPSKQUAD |
QPSK modulated signal at 50 ksymbols/second, root raised cosine filtered with an alpha of 0.35 and a 5 degree quadrature error.
|
|
|
QPSKSMRT |
QPSK modulated signal at 50 ksymbols/second, root raised cosine filtered with an alpha of 0.35 and a 1% symbol rate error.
|
|
|
QPSKSPUR |
QPSK modulated signal at 50 ksymbols/second, root raised cosine filtered with an alpha of 0.35 with a spurious signal added 36 dB below the carrier and about 11 kHz below the center frequency. |
|
RFID_EPC_Gen2_Tari25_80kbps |
RFID signal which is based on the EPCglobal Class 1 Generation 2 standard and is useful for examining Option BHC features. This signal has a forward-link Tari of 25 us, and a return link bit rate of 80 kbits/second. The data bits in this signal are a test pattern of alternating ones and zeros.
|
|
|
|
RFID_C1Gen2 |
The RFID_C1Gen2.sdf waveform is an EPCglobal C1 Gen2 Protocol (version 1.0.9) compliant signal. This signal contains two complete RF waveforms (CWs); one uses DSB-ASK modulation, while the other uses PR-ASK modulation. |
|
|
RFID_C1Gen2_QueryAck |
The RFID_C1Gen2_QueryAck.sdf waveform is an EPCglobal Class1 Generation2 forward-link signal, with a Tari of 25 us. This signal contains correct bits so that the RFID Frame Structure trace can show details of the bursts in the signal.
|
|
|
RFID_ISO14443A_106kbps
|
This is an RFID - ISO 14443 Type A standard compliant signal. The signal contains both interrogator and tag bursts. The Fwd direction uses OOK format at 106 kbits/second, the Return direction uses DSB-ASK format at 106 kbits/second. You can use the setup file (.set) to auto-configure the VSA to measure the signal. |
|
|
RFID_ISO14443B_106kbps |
This is an RFID - ISO 14443 Type B standard compliant signal. The signal contains both interrogator and tag bursts. The Fwd and Ret direction use DSB-ASK modulation format at 106 kbits/second. Line-coding is different for each, per the standard. |
|
|
RFID_ISO15693 |
This is an ISO 15693 RFID signal with both a Forward and Return burst. |
| ShapedOffsetQPSK.zip | SoqpskTg5MHz | This is a continuous Shaped Offset QPSK signal based on the SOQPSK-TG modulation format defined in IRIG 106-04 for use in telemetry. The recording is approximately 3.2 ms in length, with a center frequency of 1460 MHz, a symbol rate of 5 MHz, and a transmit filter matching the IRIG 106-04 standard. |
|
|
TD-SCDMA_TS0-1 |
TD-SCDMA waveform with both uplink and downlink pilots, as well as active channels in time slots 0 and 1.
|
|
|
TD-SCDMA_TS0-6 |
TD-SCDMA waveform with all time slots active. A number of active channels and spreading factors are present in the different traffic time slots.
|
|
|
TD-SCDMA_TS123_Mid23_NoPilots |
TD-SCDMA signal with no pilots that uses time slots 1, 2, and 3 and Basic Midamble 23. The TD-SCDMA no-pilot signal is demodulated by synchronizing to the midamble in the time slots.
|
|
TEDS_CB_100k_64Q |
TEDS signal for a Control Uplink slot format, 100 kHz channel bandwidth, and 64QAM modulation type.
|
|
|
|
TEDS_NBD_150k_64Q |
TEDS signal for a Normal Downlink slot format, 150 kHz channel bandwidth, and 64QAM modulation type.
|
|
|
TEDS_NUB_25k_16Q |
TEDS signal for a Normal Uplink slot format, 25 kHz channel bandwidth, and 16QAM modulation type.
|
|
|
TEDS_NUB_50k_16Q |
TEDS signal for a Normal Uplink slot format, 50 kHz channel bandwidth, and 16QAM modulation type.
|
|
|
TEDS_RAB Radio Access Bearer_25k_4Q |
TEDS signal for a Random Access Uplink slot format, 25 kHz channel bandwidth, and 4QAM modulation type.
|
|
3GPPDown |
Standard 3GPP W-CDMA downlink signal; Fc = 1GHz, Span = 5 MHz.
|
|
|
|
3GPPDownHSPA+ |
This is a 3GPP HSPA downlink signal consisting of 14 DPCH Dedicated Physical Channel channels and 6 HS-PDSCH High Speed Physical Downlink Shared Channel channels (2 each of QPSK, 16QAM and 64QAM). |
|
|
3GPPDownHSPA+MIMO_2ch | This is a 3GPP HSPA+ downlink 2-ch MIMO mode, over air transmission signal |
|
|
3GPPTM5H8D30 |
This is a standard 3GPP2 HSDPA High Speed Downlink Packet Access downlink signal, Test Model 5 signal.
|
|
|
3GPPUp |
Standard 3GPP2 W-CDMA uplink signal; Fc = 1GHz, Span = 5 MHz
|
|
|
3GPPUpHSPA+ |
This is a 3GPP HSPA+ uplink signal
|
|
i80216e_DL10MHz |
IEEE 802.16e downlink subframe signal using a 10MHz profile. Contains PUSC partial usage of subchannels: Some of the subchannels are allocated to the transmitter. zone (12 symbols) followed by a FUSC full usage of subchannels: All of the subchannels are allocated to the transmitter. zone (10 symbols). The i80216e_DL10MHz.set file may be used directly to setup the VSA for analysis of this recording. |
|
|
|
i80216e_DL10MHz_P2_2Ch_STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively. |
This is an IEEE 802.16e downlink subframe signal with BW=10MHz and PreambleIndex=2. It contains a PUSC zone with control information followed by another PUSC zone with Matrix A STC encoding , and a third zone with Matrix B STC encoding. The recording is made with two channels, and requires the configuration of 2-channel hardware (real or simulated) to allow playback of both channels. See Recalling Recordings. |
| WiSUN OFDM.zip |
Wisun_OFDM_Opt1_Interleaving0_3PHR |
This is an IEEE std 802.15.4g MR-OFDM signal for Wi-SUN (Wireless Smart Utility Network) with Option 1 Interleaving 0 and 3 PHR (PHY Header) symbols configured. |
|
|
Wisun_OFDM_Opt1_Interleaving1_4PHR |
This is an IEEE std 802.15.4g MR-OFDM signal for Wi-SUN (Wireless Smart Utility Network) with Option 1 Interleaving 1 and 4 PHR (PHY Header) symbols configured. |
|
|
Wisun_OFDM_Opt2_Interleaving0_6PHR |
This is an IEEE std 802.15.4g MR-OFDM signal for Wi-SUN (Wireless Smart Utility Network) with Option 2 Interleaving 0 and 6 PHR (PHY Header) symbols configured. |
|
|
Wisun_OFDM_Opt2_Interleaving1_8PHR |
This is an IEEE std 802.15.4g MR-OFDM signal for Wi-SUN (Wireless Smart Utility Network) with Option 2 Interleaving 1 and 8 PHR (PHY Header) symbols configured. |
|
|
Wisun_OFDM_Opt3_6PHR |
This is an IEEE std 802.15.4g MR-OFDM signal for Wi-SUN (Wireless Smart Utility Network) with Option 3 and 6 PHR (PHY Header) symbols configured. |
|
|
Wisun_OFDM_Opt4_6PHR |
This is an IEEE std 802.15.4g MR-OFDM signal for Wi-SUN (Wireless Smart Utility Network) with Option 4 and 6 PHR (PHY Header) symbols configured. |
|
ZigBee-2450 |
This is a burst ZigBee signal in the 2450 MHz band. |
See Also