Rn phase and Rn mag (Digital Demod)
Menu Path:
The ring identifiers (R0 - R7), mag, and phase in the symbol table (see diagram below) correspond to the Ring ID, and in the Custom APSK tab of the dialog box.
These metrics are only available when making Custom APSK measurements.
See Also