Custom APSK Tab (Digital Demod)

Menu Path: Analysis > Digital Demod Properties > Custom APSK tab

The Custom APSK tab configures constellations composed of up to 8 rings and 256 states.

Custom APSK must be selected for the Format in the Format tab of the Digital Demod Properties dialog box to make a custom APSK measurement.

The following are the parameters used to configure a custom APSK constellation:

The rings do not need to be sorted in any particular order. Any rings in the list can be disabled. This allows the Ring ID to be based on any ring, for example zero based (Ring ID "0" enabled) or one based (Ring ID "0" disabled and Ring ID "1" enabled).

The state numbering is sequential, starting at 0 on the first (lowest ID) enabled ring and proceeding down the list. The states on an individual ring start at the state denoted by the Phase for that ring and counting up counter-clockwise around the ring. This means that the state numbering on an individual ring can be rotated around the ring through the Phase entry. For example, on a 4-state ring even though the constellation would look the same for Phase entries of 45, -45, 135, -135, the first state number for that ring would be in 4 different locations.

Since the state numbering starts on the lowest Ring ID, the numbering can be started on the inner ring, the outer ring, or any other ring depending on which is the lowest Ring ID.

"Enable non-uniform phase shift definition" Check Box

The Enable non-uniform phase shift definition check box allows a different interpretation of the phase parameter under certain circumstances. The check box is available only when Ring 0 is enabled with 4 or 6 states and phase of greater than 3 degrees. When selected, the Phase parameter determines the phase rotation away from the x-axis of the 4 states that are closest to the x-axis, as shown in the diagram below. When cleared, the Phase parameter affects the constellation as described previously in this topic (rotation of a ring with evenly-spaced states).

Invalid Entries

Invalid entries will cause the Enabled checkbox to be greyed and the ring to be disabled.

See Also

Digital Demod Properties Dialog Box