Digital Demod Properties Dialog Box

The Digital Demod Properties dialog box contains parameters that configure the VSA's digital demodulator.

In the Analysis menu, Digital Demod Properties is grayed (unavailable) if the digital demodulator is not enabled. To enable the digital demodulator, click Analysis > Type > General Purpose > Digital Demod.

The dialog box contains five tabs:

See Also

Setting up Digital Demod Measurement

Selecting Digital Demod

Troubleshooting (Digital Demod)

About Digital Demodulation (Option AYA)