EDGE (Digital Demod)

This selection sets the instrument to the EDGE(3p/8 D8PSK) "Enhanced Data for Global Evolution" digital demodulation format. Use the same process to demodulate EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.) as other digital demodulation formats.

EDGE adds a new filter: EDGE(Windowed RC). Also two new digital demod error data results were added to the symbol table: Pk EVM and 95% EVM.

Use the VSA's standard preset feature to automatically configure the measurement parameters: Select the Analysis > Demod Properties > Format tab > Preset to Standard > Cellular > EDGE.

When using EDGE, note the following:

Additional Details

To learn how the VSA demodulates EDGE signals, see Digital Demodulation.

See Also

Available Digital Demodulation Formats (Digital Demod)