Preset to Standard (Digital Demod)

Menu Path: Analysis > Digital Demod Properties > Format tab

Preset to Standard selects a standard configuration for digital demodulation measurements. The VSA can be configured manually or a standard format can be selected for the digital communications system and the VSA automatically sets the configuration parameter.

See Using Standard Setups/Presets for a list of the standards supported by the VSA and the default parameter settings for those standards.

See Also

Format Tab (Digital Demod)