Format Tab (Digital Demod)
The tab configures the VSAs digital demodulator. These are the parameters necessary to lock-on to and demodulate the test signal.
Some hardware configurations may not support a span that is wide enough for the selected demod standard.
The tab parameters are:
- Preset to Standard
- Format
- Symbol Rate
- FSK Deviation Reference
- Points / Symbol
- Couple to Gain Imb. / Quad Skew
- Result Length
- Recall State Definitions
- View State Definitions
See Also
About Digital Demodulation (Option AYA)