Inst IQ Meas Spec (Digital Demod)
When is enabled, is the instantaneous spectrum of the trace. In other words, is the non-averaged versions of trace data.
The digital demodulator removes carrier frequency error. Therefore, in the error vector spectrum display, you must add the carrier frequency error to marker readouts to obtain exact frequency information. The carrier frequency error () is shown in the symbol table.
See Also