Available Error Summary Data (Digital Demod)
The Digital Demodulation determines which error summary data are displayed in the symbol table, as shown in the following table (Yes indicates the error data result is shown for that demodulation type). For a description of a particular error summary data type, click the corresponding link in the Error Summary Data column.
For information about using error summary data with ADS, see Demod Errors and ADS.
See About the Symbol Table for an overview of the symbol table. See Error Summary Data for an overview of the symbol-table error summary data.
|
Error Summary Data |
QPSK Quadrature phase shift keying, OQPSK Offset Quadrature Phase Shift Keying: A type of QPSK modulation that offsets the bit streams on the I and Q channels by a half bit. This reduces amplitude fluctuations and helps improve spectral efficiency., SOQPSK |
VSB 8/16 |
MSK Minimum Shift Keying Type 1 |
8PSK, Pi/8D8PSK, Pi/4DQPSK, |
APSK 16/32, DVB-APSK 16/32 |
Star16Qam, Star32Qam |
CPM Continuous Phase Modulation (FM Frequency Modulation) | Custom APSK | |||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
¾ |
¾ |
¾ |
¾ |
¾ |
EDGE |
¾ |
¾ |
¾ |
¾ |
¾ |
|
|
¾ |
¾ |
¾ |
Yes |
Yes |
EDGE |
¾ |
¾ |
¾ |
¾ |
¾ |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
Yes |
¾ |
Yes |
¾ |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
Yes |
¾ |
Yes |
¾ |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
2-FSK |
¾ |
¾ |
¾ |
|
|
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
¾ |
Yes |
¾ |
Yes |
|
|
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
¾ |
Yes |
¾ |
Yes |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
Yes |
¾ |
Yes |
¾ |
|
| H1, H2 |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
Yes |
¾ |
|
Yes |
¾ |
Yes |
Yes |
¾ |
Yes |
Yes |
¾ |
Yes |
¾ |
Yes |
|
|
Yes |
¾ |
Yes |
Yes |
Yes |
Yes |
Yes |
¾ |
Yes |
¾ |
Yes |
|
|
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
|
|
OQPSK, SOQPSK |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
EDGE |
¾ |
¾ |
¾ |
¾ |
¾ |
|
|
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
Yes |
¾ |
Yes |
¾ |
Yes |
|
|
¾ |
Yes |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
|
|
Yes |
¾ |
Yes |
Yes |
¾ |
Yes |
Yes |
¾ |
Yes |
¾ |
Yes |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
Yes |
¾ |
¾ |
¾ |
¾ |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
APSK 32, DVB-APSK 32 |
¾ |
¾ |
¾ |
¾ |
|
|
Yes |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
|
| Rn mag | ¾ | ¾ | ¾ | ¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
Yes |
| Rn phase | ¾ | ¾ | ¾ | ¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
Yes |
|
QPSK |
Yes |
¾ |
8PSK |
¾ |
QAM16-1024, DVB QAM |
Yes |
¾ |
Yes |
¾ |
Yes |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
2-FSK |
¾ |
¾ |
¾ |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
Yes |
¾ |
¾ |
¾ |
¾ |
|
|
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
¾ |
2-FSK |
¾ |
¾ |
¾ |