Syms/Errs (Digital Demod)
The trace is split into two sections. The upper section shows the error information and lower section shows the binary bits for each symbol. The first bit in the table corresponds to the first bit of the first symbol.
See About the Symbol Table or Available Error Summary Data for more information.
See Also