MER (DOCSIS 4.0 Upstream)
is the average value of the Modulation Error Ratio (MER) for all subcarriers in the measurement interval, expressed in decibels (dB).
A displayed value of "***", "-780dB" or "-999" means no data is available.
See Also
is the average value of the Modulation Error Ratio (MER) for all subcarriers in the measurement interval, expressed in decibels (dB).
A displayed value of "***", "-780dB" or "-999" means no data is available.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |