Available Error Summary Data (DOCSIS 4.0 Upstream)
The following table lists the available error summary results for DOCSIS 4.0 Upstream modulation analysis.
A displayed value of "***", "-780dB" or "-999" means no data is available.
Querying summary table data results programmatically
To programmatically query the Trace Summary Table data results using the Summary() and SummaryUnit() methods in the MeasurementData object.
See the How To Query Summary Table Data Results topic for more information.
See Also