OFDM Eq Ch Freq Resp (DOCSIS 4.0 Upstream)
The displays the non-averaged channel response for the specified measurement hardware.
This trace is not affected by the EQ Control settings, since EQ Control = Full is always used to compute Eq Chan Freq Resp data. It is, however, affected by the Equalizer Training selection.
The Inst Ch Frequency Response trace does not show the effects of averaging.
See Also