Syms/Errs (DVB-RCS2)

The Syms/Errs trace is split into two sections. The upper section shows the error information and lower section shows the binary bits for each symbol. The first bit in the table corresponds to the first bit of the first symbol.

See Error Summary Data for more information.

See Also

Available Symbol Table Error Summary Data