Meas Decoded Bits (DVB-S2/S2X)

The Meas Decoded Bits trace shows the decoded bits for the physical layer channels.

The level of encoding is determined by the BCH/LDPC Encode On parameter.

By default, the bits are displayed in 8-bit bytes in hexadecimal format. Like other bit displays in the VSA software, Trace > Properties > Digital Demod > Symbol Table Format can be used to switch from hex to binary.

 

See Also

Available Trace Data