Also Auto-detect AQPSK (GSM/EDGE/EDGE Evolution)
Cleared
specifies whether to detect AQPSK constellations when Modulation Scheme is set to .
This parameter is cleared by default since modulation can be difficult to distinguish from the other modulation schemes for certain values of the AQPSK Subchannel Power Imbalance Ratio parameter.
See Also
AQPSK Subchannel Power Imbalance Ratio