TSC Index (GSM/EDGE/EDGE Evolution)
Automatic
TSC Indexsets the Training Sequence Code index of the current burst. The current burst is determined by the Timeslot parameter. The TSC Index can be or .
For AQPSK modulation, sets the training sequence code for Subchannel A.
When is selected, the measurement will demodulate the first matching the Modulation Scheme and Timeslot parameters and auto-detect the TSC Index of that .
When is selected, the measurement will demodulate the first matching the specified , , and parameters. The range for the TSC Index is 0-7.
See Also