Timeslot (GSM/EDGE/EDGE Evolution)
Automatic
Timeslotspecifies the slot to demodulate. Timeslot can either be or .
When is selected, the first slot matching the parameters TSC Index and Modulation Scheme parameters on the Format tab will be demodulated.
When is selected, the slot specified in the box will be demodulated. The range of the slots is 0-15.
Slots are numbered starting with slot zero which is the first complete slot in the Search Time data.
The current is displayed in the Time trace.
See Also