Selecting GSM/EDGE/EDGE Evolution Demodulation

GSM/EDGE/EDGE Evolution Modulation Analysis configures the 89600 VSA to demodulate GSM Global System for Mobile Communications: Originally developed as a pan-European standard for digital mobile telephony, GSM has become the world’s most widely used mobile system. It is used on the 900 MHz and 1800 MHz frequencies in Europe, Asia and Australia, and the 1900 MHz frequency in North America and Latin America., EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.), or EDGE Evolution signals.

To select the GSM/EDGE/EDGE Evolution demodulator, click Analysis > Type > Cellular > GSM/EDGE/EDGE Evolution.

Example recordings

The 89600 VSA includes several example signals that can be used to help you learn how to use the GSM/EDGE/EDGE Evolution demodulator. The included signals are listed in the Demo and Recorded Signals topic in the Getting Started book.

See Also

Setting up a GSM/EDGE/EDGE Evolution Measurement

Using Standard Setups/Presets

Troubleshooting

Available Features

About GSM/EDGE/EDGE Evolution Modulation Analysis (Opt AYA)