Spectrum (GSM/EDGE/EDGE Evolution)
The trace displays the averaged frequency spectrum of the data from the Time trace. When averaging is OFF, the and Inst Spectrum traces are identical, as shown in the following block diagram (the block diagram is part of the Digital Demodulation Block Diagram).
The trace has the following characteristics:
- Derived from pre-demodulated time data, which is 25% longer than the that is demodulated.
- Averaged when averaging is ON and the average type is , , or averaging.
When averaging is ON, a scan is not included in the average when any of these conditions exist: Pulse Not Found, Sync Not Found, Carrier Unlock.

See Also