About Per-Carrier Trace Types (Flex Frame)
There are two types of traces in the Trace > Data > Demod menu that display component carrier data:
-
CCn - A menu of demod traces will appear for each component carrier configured in the Carrier Aggregation tab. When a trace is selected from a CCn menu, "CCn" will be shown in the trace's title to indicate that the data displayed in the trace is specific to that component carrier. The component carrier will not change with this type of demod trace, regardless of the Display parameter's CC selection.
-
Display CC - Traces in this menu display demod data for the component carrier selected by the Carrier Aggregation tab's Display parameter. This type of trace provides a means of configuring a single set of traces and switching between measured component carriers using the Display parameter. When a trace is selected from the Display CC menu, "(CCn)" will be shown (enclosed in parentheses) in the trace's title to indicate that the data displayed in the trace will dynamically change depending on the Display parameter selection.
See Also