Carrier Aggregation Tab (Flex Frame - Advanced Mode)
The tab configures component carriers and their channel assignments.
Aggregation combines up to 16 component carriers into a single signal. The Carrier Aggregation feature allows you to define and simultaneously analyze multiple carriers. Each carrier can have different allocations, measurement parameters, and even symbol rate.
The Carrier Aggregation tab configures these parameters:
- Reference Frequency Mode
- Reference Frequency
- Enabled
- Name
- Absolute Center
- Offset
- Symbol Rate
- Assigned Channels
- Copy CCn to...
- Duplicate Carrier (icon)
- Remove Carrier (icon)
- Add CC
See Also
Flex Frame Properties Dialog Box