CDF (Flex Frame)

CDF shows the cumulative distribution function for the data in the measurement interval. CDF Cumulative Distribution Function: The cumulative probability that a parameter will be less than a given value X. shows the probability that the voltage of a random data sample (x) will be less than K volts, where K is a value on the x-axis.

CDF(K) = Probability(x £ K)

The CDF is computed by integrating the PDF (Probability Density Function).

This trace can be useful in designing an amplifier for a particular type of signal. For example, for an amplifier that saturates at 212 mV, you can place a marker at 212 mV to find what percentage of the time the signal is below the saturation level.

This trace will continue to accumulate data until the measurement is restarted.

For more information, see the CDF trace topic in the Reference.

See Also

PDF

CCDF

Available Trace Data