Starting and Stopping a Measurement
in the Control toolbar.
is available from the menu or as a button,
in the Control toolbar.
is available only from the menu.
Clicking
clears existing data and starts a new measurement. Clicking stops the current measurement and clears existing data.If the VSA is already making a measurement, clicking
clears all measurement data from the VSA's buffers and starts the measurement over again. This differs from the action of , which does not clear the buffers.The measurement control buttons in the toolbar or in the selected measurement. To start or pause multiple measurements, use the buttons on the Measurements dialog.
menu only apply to theOperation With Single Sweep
If
sweep is selected ( ), then clicking clears measurement data and performs a single sweep. To initiate a measurement without clearing measurement data, click .Operation With Trigger
Clicking
does not provide a trigger signal. To enable triggering, click and select an appropriate trigger option from the dialog box.Operation With Averaged Measurements
The operation of Pausing and Single-Stepping a Measurement.
remains the same for averaged measurements. If the averaged measurement is collecting averages, clicking starts a new averaged measurement, beginning with the first average. For information about averaging behavior when pausing/single-stepping the measurement, seeSee Also
Disconnecting from Measurement Hardware
Pausing and Single-Stepping a Measurement
Configuring Measurement Sweep Mode
Configuring Multiple Measurements