Eq Impulse Response (Flex Frame)

There are two types of traces in the Trace > Data > Demod menu that display component carrier data: CCn (component carrier is fixed), and Display CC (component carrier is dynamically selected using the Carrier Aggregation > Display parameter). See About Demod Per-Carrier Trace Types for more information.

When Digital Demod is enabled and the equalizer is ON, the Eq Impulse Response trace shows the impulse response of the equalization filter for the component carrier.

See Also

Available Trace Data