Inst Error Vector Spectrum (Flex frame)
There are two types of traces in the Trace > Data > Demod menu that display component carrier data: CCn (component carrier is fixed), and Display CC (component carrier is dynamically selected using the Carrier Aggregation > Display parameter). See About Demod Per-Carrier Trace Types for more information.
The trace shows the instantaneous spectrum of the trace. This is the non-averaged Error Vector Spectrum trace data.
The center frequency and span for is identical to the IQ Meas Spectrum.