Measurement Pause Enable

Analysis > FMCW Radar Properties > Advanced

When Measurement Pause Enable is checked, you can a configure a conditional logic test to be performed on one of the supported FMCW Region Table result metrics after each measurement update.

The conditional logic test is applied to each detected region within the FMCW Region Table results, which matches the specified Reference Region. If the conditional logic test condition is met for any one of the valid detected regions, the measurement will revert to the Control, Pause state, with the current acquisition signal data and FMCW region analysis results available on screen for further troubleshooting.

In this way you have the ability to capture and pause for further analysis specific performance or impairment results of interest, even for sporadic / intermittent events.

See Also

Reference Region