Trend/Histogram Enable

Analysis > FMCW Radar Properties > Advanced

Allows you to enable or disable all Trend/Histogram data gathering and trace results. You can specify whether Mean, Slope, or Second Order fit should be removed from the Trend and Histogram results.

When Trend / Histogram Enable is checked, FMCW Region Table result metrics from subsequent measurement updates will be included within the accumulated Trend and Histogram statistical data set.

When Trend / Histogram Enable is unchecked, FMCW Region Table result metrics from subsequent measurement updates will be excluded from the accumulated Trend and Histogram statistical data set.

Changing the state of the Trend / Histogram Enable checkbox while performing continuous measurement updates does not reset the accumulated Trend and Histogram statistical data set. The accumulated Trend and Histogram statistical data can be reset by restarting the measurement.

See Also

Remove Slope

Remove Second Order

Remove Mean

Display Length (Trend/Histogram)

Internal Buffer Length

Histogram Range