Extra Acquisition

Analysis > FMCW Radar Properties > Time

Specifies the number of extra acquisition samples reported before the start of the first valid detected FMCW region result, and after the end of the last valid detected FMCW region result. This affects how many additional display samples are made available for viewing within the synchronized Amplitude, Phase, FM Frequency Modulation and FM Slope versus time trace results.

Increasing the number of Extra Acquisition samples may be required to allow automatic time alignment of user Selected Regions to the 10% to 90% time trace grid graticules when Include Extra Data Before and After is enabled.