Include Extra Data Before and After

Menu Path: Analysis > FMCW Radar Properties > Time

When Include Extra Data Before and After is checked, display of the user Selected Regions within the synchronized Amplitude, Phase, FM Frequency Modulation and FM Slope versus time trace results will be automatically time aligned to the graticule 10% to 90% x-axis grid lines. This allows you to view measured data samples before and after the Selected Regions of interest (as shown below for first 4 detected regions).

Increasing the number of Extra Acquisition samples may be required to support automatic time alignment of user Selected Regions to the graticule 10% to 90% x-axis grid lines when Include Extra Data Before and After check-box is enabled. This is especially the case when viewing a large number of Selected Regions.

When Include Extra Data Before and After is unchecked, display of the user Selected Regions within the synchronized Amplitude, Phase, FM and FM Slope versus time trace results will be automatically time aligned to the graticule 0% to 100% x-axis grid lines.